REGEN.POWER
Description
This parameter reads regen resistor's calculated power, which is determined as follows:
(V2 / R) * DutyCycle
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Watt |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
REGEN.POWER | 0x3007 | 0x2 | UDINT | - | - | RO | True |
|
Copyright © 2018 Kollmorgen |
|